2601_MTN6705-0008S_MTN6805-0008_SW

About the Document

Document Scope

This document describes the Switch Blind Secure software application 5810/1.1. The software application is designed to program the SpaceLogic KNX, Secure, Switch/Blind Master.

You can add up to two Switch/Blind extensions to the device. Together with the two extensions, up to 24 switching outputs are available. Two switching outputs can be configured as blind/roller shutter outputs.

The basic settings of the device are set on the General settings tab. Here you define the device configuration from master and extensions. You can then also specify the functions of the outputs here.

General Settings

The functions of the outputs are parameterized on the Express settings and Extended settings tabs of the outputs for switching, roller shutter and blind.

Express Settings for Switching

Express Settings for Blind/Roller Shutter

Extended Settings for Switching

Extended Settings for Blind/Roller Shutter

You can use the Extended settings of the device to configure the global settings of the devices as needed. (Extended Settings).

Validity Note

The information contained in this guide is accurate and applicable as of the publication date. Any updates or changes to the software application will be documented in subsequent revisions of this guide. Users are advised to refer to the latest version of the user guide for the most current information.

The device is commissioned using KNX-certified software. The application and the technical descriptions are updated regularly and can be found on the Internet. This application runs in conjunction with ETS software version 5 or higher.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Product Related Cybersecurity Information

KNX Data Secure

The KNX standard has been extended by KNX Data Secure to protect KNX installations from unauthorized access. KNX Data Secure reliably prevents the monitoring of communication and manipulation of the installation. KNX Data Secure describes the encryption at telegram level so that communication via objects is encrypted and therefore secure.

Encrypted telegrams are longer than the previously used unencrypted telegrams. For secure programming via the KNX bus, it is therefore necessary for the interface (e.g. USB) and any line couplers to support these „KNX long frames“.

Special conditions must be observed when using secure devices in the ETS. Please refer to the relevant web pages on the KNX website https://www.knx.org

Protecting your data is a top priority. Use the options in the ETS and KNX Data Secure to protect your data, configuration and installations from unauthorized access.


Protecting the Project Configuration via the ETS

In the ETS, you can define a project password that protects the devices and configuration data from unauthorized access.

  1. Find your project in the Overview tab of the ETS.

  2. Click the Details > Security > Add device certificate and set your project password.

    NOTE: A good password should consist of at least 8 characters in the project window, consisting of a number, an upper case letter, a lower case letter and a special character. Never use weak PIN codes, e.g., 1234, 0000.

  3. Scan or enter the device certificates for all devices in your project that you intend to download using secure commissioning > click OK

    NOTE: The certificate consists of the serial number and the security key FDSK (Factory Default Setup Key). The FDSK is only used for initial commissioning and is replaced by the ETS during the first download. This prevents unauthorized persons from gaining access to the installation despite knowing the FDSK.
    The FDSK is printed on the device label both as a QR code and in text form.


Background information on the encryption process

  • Read or enter the FDSK into the ETS.

  • The ETS then generates a device-specific tool key.

  • When configuring the device, the ETS sends the tool key to the device. The transmission is encrypted and authenticated with the FDSK.

  • From this point on, the device only accepts the tool key for communication and the FDSK can only be used to reset the device to the delivery status. All safety-relevant data is deleted during this reset. Therefore, please keep the FDSK in your project documents.

  • The ETS then generates runtime keys, which are required for protected group communication. The transmission is encrypted and authenticated with the tool key.

Available Languages of the Document

The document is available in these languages:

  • English

  • French

  • German

  • Spanish

Related Documents

Title of documentation

Reference number

SpaceLogic KNX, Secure, Switch/Blind Master, Installation and Connection

MTN6705-0008S_HW

To find documents online, visit the Schneider Electric download center (www.se.com/ww/en/download/).

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Trademarks

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?