2601_MTN6705-0008S_MTN6805-0008_SW

Activación de los ajustes ampliados para persiana/persiana enrollable

Maestro / Ext. 1/2

Salida 1+2 / 3+4 / 5+6 / 7+8

-Persiana/persiana enrollable

Ajustes exprés para persiana/persiana enrollable

 

Ajustes ampliados para persiana/persiana enrollable

No

Para activar los ajustes ampliados para persiana/persiana enrollable, debe desbloquearlos aquí.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?