D3349890_03

Type of Moments

There are three types of moments in the app:

Types of Moments

Parameters

Editable in app

Display

Manager Scenes

  • Linked to scene widget in Manager visualization

  • Displayed, controllable, located in the Moments screen in the Automations tab.

No

  • No icons or edit options in the app

C-Bus Scenes

  • Created in the controller (using Configurator).

  • Centralized.

  • Mapping exists only between scene actions and C-Bus group objects.

  • Logic is evaluated in the controller.

No

Tap to display controller scenes in the app (green icon).

Tap to hide controller scenes in the app (black icon).

NOTE: The house icon is displayed even if no controller scenes are available. It is just not functional.

Moments

  • Created in mobile app

  • Composed of devices.

  • Stored and evaluated in the controller.

Yes

  • Custom icon and edit options displayed.

  • You can create and edit them in the app.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?