D3349890_04

General Lighting Dimmer

The General Lighting Dimmer widget is used for level control of a load (from 0% to 100%). The Ramp rate is associated with the On/Off button.

To configure General Lighting Dimmer:

  1. In General tab, enter the Title of the widget, Light titles, and Ramp Rates.

  2. In Objects tab, select the Value objects for the General Lighting Dimmer from the drop-down.

    General Lighting Dimmer supports the following type of objects:

    • Lighting applications

      • Legacy Lighting

      • Dimmer

    • If only one dimmer channel is selected, the widget looks as shown below.

    • If more than one dimmer channel is selected, the widget looks as shown below.

      All the dimmer channels can be configured separately by providing names for each channel and they can be controlled using these widgets.

      • Click Tap to turn off or big bulb icon to control all switch on/off in group.

        Group dimming can be done using the slider.

      • Click individual small bulb icon to on/off the individual loads.

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.