D3349890_04

Alarm Panel

The Alarm Panel widget is used to monitor and control C-Bus enabled security systems.

IMPORTANT: The Alarm Panel widget will support any security panel that has implemented C-Bus security application.

You can:

  • Emulate a remote security keypad

  • Disarm the security system

  • Set the security system mode

  • Monitor active alarms and system status

  • Track the status of individual security zones

View Alarm Panel

Manager Config enables you to manage all configurations for the Alarm Panel widget. In mobile app, you can view the status of each alarm or zone whether they are triggered or cleared.

  1. In the Home screen, tap Security.

    NOTE: Security is visible only if your alarm panel is connected to the controller. The Alarm Panel widget is created in Manager Config.

    The Alarm Panel Security screen appears.

    The Armed screen appears only when a security code has been set and Alarm Panel widget is locked.

  2. Enter your security code using the keypad and tap Enter to disarm the Alarm Panel widget. The Quick Function screen appears.

  3. Tap on the desired function, a C-Bus message is automatically sent to trigger the corresponding quick function.

  4. Tap Alarms tab. You can view the configured alerts and its status.

    The below table represents the overview of alarm status and active alerts.

    Alarm status: Clear Alarm status: 1 alarm triggered

    Green color in the widget indicates your home is armed.

    Grey color in the widget indicates your home is disarmed.

    The panel displays the Alarm status, indicating how many alarms have been triggered.

    Refer the below table for color indicators:

    Amber indicates that alert is triggered.

    Green indicates that no alert has been triggered.

  5. Tap Tap to see more in View Keypad widget to navigate to Alarm Panel (Armed) screen.

  6. Tap Tap to see more in Quick Action widget to navigate to Alarm Panel (Disarmed) screen.

  7. You can either:
    • Tap Zones widget to open the Zones section.

      or

    • Tap Zones tab.

      You can view the zones that are configured in Manager Config.

      The below table represents the overview of zone status, alarm indicators and active zone alerts.

      Zone status: 2 zones triggered

      Zone status: Clear

      The panel displays the Zone status, indicating the number of triggered zones.

      Clear status indicates that no zones are currently triggered.

      Refer the below table for color indicators:

      Amber indicates that zone is triggered.

      Green indicates that no zone has been triggered.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.