D3349890_04

Shutter Relay Horizontal

The Shutter Relay Horizontal widget enables the operation of electric curtains, blinds, and shutters.

Shutter Relay Horizontal has three key function which allows to open, close, and pause the electric curtains, blinds, and shutters.

It has dual-control functionality which enables to handle both blinds and shades together. Shutter and blinders can be controlled individually using slides.

To control On/Off for both shutter and blinds together use (<) and (>) buttons.

To configure Shutter Relay Horizontal:

  1. In General tab, enter the Title of the widget.

    Click the Invert movement check box, to invert the control options configured for the nudge buttons.

  2. In Objects tab, select the Shutter/blind block out object and Shutter/blind shade object for the Shutter Relay Horizontal from the drop-down.

    Shutter Relay Horizontal supports the following type of objects:

    • Lighting applications

      • Legacy Lighting

      • Shutter/Blind Level

    NOTE: Blockout object is required, and shade object is optional.
  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.