D3349890_04

Rename Device

Renaming your device allows you to identify it, especially if you have multiple devices connected to your app.


To change the device name:

  1. Tap > Devices > tap on the device name.


    Rename Device page appears.
  2. Enter a new name.

  3. Tap Save . The new device name is saved.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.