D3349890_04

Lighting Preset

The Lighting Preset widget is used for setting a load to a preset level (from 0% to 100%).

The appearance of the widget depends on the number of labels created for an individual object. Minimum one label has to be created, and maximum three labels.

NOTE: Only one preset level can be set at a time.

Lighting Preset with 1 label

NOTE: If any of the configured preset value is not currently set or active, the widget is displayed in an off state.

To configure Lighting Preset:

  1. In General tab, enter the Title of the widget, preset labels and respective values (0 - 255), and ramp rates (0 sec – 17 min).

  2. In Objects tab, select the Value object for the Lighting Preset from the drop-down.

    Lighting Preset supports the following type of objects:

    • Lighting applications

      • Legacy Lighting

      • Dimmer

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click the Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.