D3349890_04

Scene Trigger

Scene Trigger widget is used for setting a scene which allows many lights to be set to predetermined levels all at once.

To operate the scene trigger:

  1. Click on the desired scene in the widget.

    NOTE: Only one scene can be set at a time.

Example: You can set up a Morning Routine scene in your smart home system.

This scene is designed to:

  • Turn on the bedroom lights to a gentle, warm setting.

  • Reduce the Fan speed.

  • Open the electric blinds or curtains to let in natural light.

To use the Scene Trigger widget for this scenario, you can:

  • Place the Morning Routine scene trigger widget on your home screen for easy access.

  • When you wake up in the morning, you can simply tap the Morning Routine button on the widget.

    NOTE: Instantly, all the predefined actions associated with the Morning routine scene are executed, creating a pleasant and seamless morning routine without the need to manually control each device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.