D3349890_04

General Lighting Dimmer

The General Lighting Dimmer widget is used for level control of a load (from 0% to 100%).

The functions supported by the widget are:

To operate the General Lighting Dimmer:

  1. Click anywhere on the widget to On/Off the individual dimmer channel.

    NOTE: Use level slider to increase /decrease the level.
  2. Click on the large bulb icon to On/Off the group dimmer channels.

  3. Click on the small bulb icon (small individual dimmer channel) to control individual dimmer channel among the multiple dimmer channels.

    NOTE: Individual dimmer channel can only perform On/Off. Use level slider to increase /decrease the level for group dimming.

Single dimmer On State

On State

Off State

Example: You can use the General Lighting Dimmer widget to create a night light effect, providing just enough light for comfort without being too bright.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.