D3349890_04

General Switch

A General Switch widget is used to On/Off the individual loads.

To configure General Switch:

  1. In General tab, enter the Title of the widget.

  2. In Objects tab, select the Switch object for the General Switch from the drop-down.

    General Switch supports the following type of objects:

    • Lighting applications

      • Legacy Lighting

      • Switch

      • Up/Down

      • Open/Close

      • Boolean

      • Dimmer

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.