D3349890_04

General Switch

General Switch widget allows you to switch between On and Off using the on/off functions.

  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the General Switch.

  3. Tap on the widget to operate the General Switch.

    The General Switch screen appears.

On State

Off State

Example: You can use the General Switch widget to turn lamps or overhead lights on and off remotely.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.