D3349890_04

Shutter Relay Horizontal

Shutter Relay Horizontal widget is used to operate electric curtains, blinds, and shutters.
  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the Shutter Relay Horizontal.

  3. Tap on the widget's label. The Shutter Relay Horizontal screen appears.

    • You can control the open/pause/close functions.

    • Tap to pause the curtain.

    • Tap to close the curtain.

    • Tap to open the curtain.

Shutter Blockout Closed

Shutter Blockout Open

Shutter Shade Open

Shutter Shade Closed

Example: If you have shutters installed in your home and you have set up a Shutter Relay widget in your smart home system, you can conveniently open or close the shutters with a tap on the widget.

For instance, if you want to close the shutters in the evening for privacy and security, you can use the Shutter Relay widget to send a command that closes the shutters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.