D3349890_04

Info 2

Info 2 widget is used to display the error messages/trigger messages (values or data of the object assigned).

To configure Info 2:

  1. In General tab, enter the Title of the widget, Text 1 and Text 2 description.

  2. In Objects tab, select the Text 1 and Text 2 objects for the Info 2 from the drop-down.

    Info 2 supports the following type of objects:

    • Error Application

    • User Parameter

      • Boolean

    • Trigger Application

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.