D3349890_04

Info 1

Info 1 widget is used to display the values of the object assigned.
  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to view the information.

Example: You can use the Info 1 widget to display the current indoor or outdoor temperature, and to display reminders for daily tasks or important events.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.