D3349890_04

Scene Trigger

The Scene Trigger widget is used to set a scene, enabling the adjustment of multiple lights to predetermined levels simultaneously.
  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the scene.

  3. Tap on SET SCENE, to activate a scene in the Scene Trigger widget. This action will then set the corresponding values in the controller.

Before Triggering

After Triggering

Example: You can set up a Morning Routine scene in your smart home system.

This scene is designed to:

  1. Turn on the bedroom lights to a gentle, warm setting.

  2. Reduce the fan speed.

  3. Open the electric blinds or curtains to let in natural light.

To use the Scene Trigger Widget for this scenario, you can:

  1. Place the Morning Routine scene trigger widget on their home screen for easy access.

  2. When you wake up in the morning, you can tap on the Morning Routine button on the widget.

  3. Instantly, all the predefined actions associated with the Morning Routine scene are executed, creating a pleasant and seamless morning routine without the need to manually control each device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.