D3349890_04

Configure Widgets

Each widget added in the rooms can be configured individually according to user requirements.

Widgets are categorized based on the following function types:

Function Type

Widgets

Lighting

  • Light Switch

  • Socket Switch

  • General Switch

  • Lighting Switch

  • General Lighting Timer

  • General Lighting Dimmer

Climate

  • Fan Controller

  • Fan Switch

  • AC Switch

  • AC Control Unit

  • Zone Control

General

  • Info 1

  • Info 2

  • Bellpress

  • Enable Preset

  • Two-State Enable

Blinds

  • Change Over Relay

  • Shutter Relay Horizontal

  • Shutter Relay Vertical

Scenes

  • Local Scene Controller

  • Scene Trigger

Other widget

Alarm Panel

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.