D3349890_04

Enable Preset

Enable Preset widget is used to enable the preset level.

Enable Preset widget allows you to create either one or more preset labels (maximum 3).


To operate the Enable Preset:

  1. Click on any of the preset label to turn On.

    NOTE:
    • Only one preset level can be set at a time.

    • If any of the configured preset value is not currently set or active, the widget is displayed in an Off state.

On State

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.