D3349890_04

Schedulers

Scheduler provides control of different lighting functions using date and time.

Scheduler feature is supported for the following widgets:

  • Light Switch

  • General Switch

  • Socket Switch

  • Fan Switch

  • AC Switch

  • General Lighting Dimmer

  • Shutter Relay Horizontal

  • Shutter Relay Vertical

To set the scheduler for a widget:

  1. Click to unlock the widgets.

  2. Click ellipse icon of the widget.

  3. Click Schedulers > Add scheduler.

  4. Enter the Schedule name and Notes (if required).

  5. Select the Schedule timeframe as per the requirement.

    • Hourly: Select the minutes you want to run scheduler.

    • Daily: Select the hour:minute you want to run scheduler.

    • Weekly: Select the day(s), and hour:minute you want to run scheduler.

    • Monthly: Select the month(s), day(s), and hour:minute you want to run scheduler.

    • Yearly: Select the month(s), date(s), and hour:minute you want to run scheduler.

  6. Select the Item check box to add the scheduler for selected item. It displays the item for which schedulers can be added.

  7. Set desired value for the scheduler using Item value slider.

  8. Select the seconds to be set using ramp rate drop-down.

  9. Click Take actual value to retrieve current value of the item.

  10. Click Toggle scheduler active to activate the scheduler.

  11. Click Save scheduler to save the scheduler details.

  12. Click Cancel scheduler to cancel the operation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.