D3349890_04

General Lighting Timer

The General Lighting Timer widget is used for switching on a load for a specific period.

To start the timer, click on the Start button and set the target level. A second click, stops the timer and sets the return level.

If left running, the return level will be set at the end of the period using the ramp rate (if defined).


To configure General Lighting Timer:

  1. In General tab, enter the title of the widget, Target Level (%), Ramprate Target (sec), Return Level (%), Ramprate Return and the time duration.

  2. In Objects tab, select the Value Object for the General Lighting Timer from the drop-down.

    General Lighting Timer supports the following type of objects:

    • Lighting applications

      • Legacy Lighting

      • Boolean

      • Switch

      • Up/Down

      • Alarm

      • Boolean

      • Open/Close
      • Start/Stop

      • High/Low

      • Enable

      • Invert Enable

      • Boolean Inversion

      • Boolean Boolean

      • BellPress

      • Dimmer

      • Shutter Blind

      • Shutter Blind Level

      • Cycle Fan

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

    NOTE: The mobile application will not support the General Lighting Timer, this feature is limited to the Manager interface.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.