D3349890_04

Fan Controller

The Fan Controller widget is used to control the speed of a fan.

Fan Controller has different predefined modes set with different speed.

The functions supported by the widget are:

  • On

  • Off

  • Modes : Slow/Medium/Fast

To operate the Fan Controller:

  1. Click anywhere on the widget to turn on.

  2. Click (<) or (>) buttons to change the fan mode/speed.

  3. Click (>) button to turn off the fan.

    NOTE: When turned on, by default it is in first (slow) mode.

Off State

On State

Example: For the hall, you can use the Fan Controller widget to set the fan speed to fast/medium/slow. Whether you want a refreshing breeze or a gentle airflow, the Fan Controller helps you maintain the perfect atmosphere.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.