D3349890_04

Two-State Enable

The Two-State Enable widget is used to set the state of a load.

To configure Two-State Enable:

  1. In General tab, enter the Title of the widget, State Label and respective State Value.

  2. In Objects tab, select the Value object for the Two-State Enable from the drop-down.

    Two-State Enable supports the following type of objects:

    • Lighting applications

      • Legacy Lighting

      • Switch

      • Up/Down

      • Open/Close

      • Boolean

      • Dimmer

      • Enable

      • Invert Enable

      • High/Low

      • Start/Stop

      • Boolean Boolean

      • Boolean Inversion

    • Enable Application

    • Trigger Application

    • User Parameter

      • Boolean

      • Signed

      • Unsigned

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.