D3349890_04

Socket Switch

A Socket Switch widget is used to switch On or Off the individual loads.

To configure Socket Switch:

  1. In General tab, enter the Title of the widget.

  2. In Objects tab, select the Switch object for the Socket Switch from the drop-down.

    Socket Switch supports the following type of objects:

    • Lighting applications

      • Legacy Lighting

      • Switch

      • Up/Down

      • Open/Close

      • Boolean

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click the Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.