D3349890_04

Scene Trigger

The Scene Trigger widget is used for setting a scene which allows multiple lights to be set to predetermined levels all at once.

Scene Trigger allows to create a minimum 1 scene, and maximum 6 scenes.

To configure Scene Trigger:

  1. In General tab, enter the Title of the widget, Scene name and value.

  2. In Objects tab, select the Scene object for the scene from the drop-down.

    Scene Trigger supports the following type of object:

    • Trigger Application

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

    NOTE: When a scene is created in Configurator and then added as a widget in Manager, the mobile app will display 2 moments with the same scene. One moment uses the scene name from Configurator and other moment uses the scene name defined in the scene widget in Manager.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.