D3349890_04

Installing Apps into Controller for Cloud Connectivity

This section explains how to install apps into controller for cloud connectivity.

  1. On Home page, click to open configure apps page.

  2. In the configure apps page, click on to install the apps.

  3. Install the Cloud connector, IoT third party API, Management and Manager visualization applications in the C-Bus controller that allows the automatic update of the applications. (If Manager is already downloaded, you can download only Cloud connector, and IoT third party API )

NOTE: It is recommended to allow automatic updates of Cloud Connector, IoT third party API applications, Management and Manager. So you won't have to manually update the applications in the Cloud Marketplace in the future.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.