D3349890_04

Lighting Preset

The Lighting Preset widget allows you to establish the load at a predetermined level ranging from 0% to 100%. This widget also supports the set level function for added convenience and control.

  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the Lighting Preset.

  3. Tap on the widget's label to operate the Lighting Preset.

    The Lighting Preset screen appears.

NOTE: If any of the configured preset value is not currently set or active, the widget displays in an off state.

On State

Off State

Example: You can set Lighting Preset widget with different labels :

  • Work Mode: Set a bright, cool lighting preset for your home office to help you stay alert and focused during work hours.

  • Relaxation: Create a preset with soft, dim lighting for relaxation or meditation sessions which can help to unwind after a long day.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.