D3349890_04

Widget Configuration

You need to configure the widgets in the Manager application properly to control your device through the Clipsal C-Bus manager mobile app. The following table describes which widget to use for the required functionality and which mandatory parameters and group objects you need to configure.

NOTE: Any changes in the configuration will take time to show up in the mobile app. You can wait for a minimum of one minute before refreshing.

Lighting

Light Switch

General Switch

Socket Switch

General Lighting Dimmer

Lighting Status

Lighting Preset

Blinds

Change Over Relay

Shutter Relay Vertical

Shutter Relay Horizontal

Climate

Fan Switch

AC Switch

Fan Controller

AC Control Unit

Zone Control

Scenes

Scene Trigger

Local Scene Controller

General

Info 1

Info 2

Bellpress

Enable Preset

Two-State Enable

Other Widgets

Alarm Panel

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.