D3349890_04

Two-State Enable

Two-State Enable widget is used to set the state of a load.

The functions supported by the widget are:

  • On/Off

  • Enable/Disable

To operate the Two-State Enable:

  1. Click On or Off on the widget respectively to turn On/Off.

On State

Off State

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.