D3349890_04

Moments

You can create a moment to change the state of several devices with single tap.

Moments are created and edited in the Automations section.

  1. On the Home screen (Home Screen), tap .

  2. Select the Moments tab.

    NOTE: A moment will only set the status of devices. To transition the affected devices to a different status, you must either change it manually or create a reversing moment.

The widgets supported by the Moment are Light Switch, General Switch, Socket Switch, General Lighting Dimmer, AC Switch, Fan Switch, Shutter Relay Vertical, and Shutter Relay Horizontal.

NOTE: If a scene is created in both the Configurator and the Manager Config, 2 moments for the same scene will appear in the mobile app.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.