D3349890_04

Fan Controller

The Fan Controller widget is used to control the speed of a fan.

The Fan Controller has various predefined modes with different speeds. The functions supported by the widget include on/off functionality and mode selection.

Example: Slow/Medium/Fast

  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the Fan Controller.

  3. Tap on the widget's label. The Fan Controller screen appears.

    • Tap to turn on the Fan Controller.

    • Tap twice to increase the fan speed.

    • Tap to decrease the fan speed and to turn off the Fan Controller.

Off State

On State

Example: For kitchen ventilation, you can use the Fan Controller widget to set at medium speed while cooking to help ventilate the kitchen and remove cooking odors.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.