D3349890_04

Info 2

Info 2 widget displays the values of the object assigned.

Example: You can use the Info 2 widget to display the error message from the various devices configured.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.