D3349890_04

Firmware Update

Follow the below steps to update the firmware:
  1. Go to https://www.se.com/au/en/search/?q=5500ac2.
  2. On the page, scroll down to the Software and Firmware section.
  3. Click the firmware file (the highest available version) that corresponds to your hardware version.
  4. In the C-Bus controller, access the Configurator (accessible only with the Administrator account).
  5. Click ˃ System tap at the top left ˃ Upgrade firmware.
  6. In the pop-up window, click Choose File and select the file downloaded in step 3.
  7. Click Open and update the firmware. Once done, the controller automatically reboots.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.