D3349890_04

Info 1

Info 1 widget is used to display the values of the object assigned.

Example: You can use the Info 1 widget to display the current indoor or outdoor temperature, display reminders for daily tasks or important events.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.