D3349890_04

Creating Manager Visualization

Manager is an application that allows you to control the C-Bus devices through a widget-based visualization. It also provides the inputs for the Clipsal C-Bus manager mobile app.

With Manger Config application, the system integrator designs a visualization as follows:

  1. Log in to your controller and download the Manager app from the cloud Marketplace (see Installing Apps into Controller for Cloud Connectivity).

  2. On the Start page, click Manager Config to open the visualization configurator Main screen.

  3. Click ADD NEW FLOOR at the bottom of the page and name your floor. For more information, refer section Add a Floor.

  4. Click ADD NEW ROOM and name your room. For more information, refer section Add a Room.

  5. Click ICON and assign it to your rooms.

  6. Click ADD NEW WIDGET and add widgets to your rooms. For more information, refer section Add a Widget.

    NOTE: You have the ability to accelerate visualization deployment by duplicating your rooms. This allows for copying rooms, along with all widgets and this process maintains the preservation of the room and widget.

    The C-Bus objects mapping have to be changed according to your installation.

    Learn more on creating Manager visualization: Manager Config.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.