D3349890_04

Shutter Relay Vertical

Shutter Relay Vertical widget is used to operate electric curtains, blinds, and shutters.
  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the Shutter Relay Vertical.

  3. Tap on the widget's label. The Shutter Relay Vertical screen appears.

    • You can control the open/close/pause functions.

    • Tap to close the shutter.

    • Tap to open the shutter.

    • Tap to pause the shutter.

Shutter Blockout Closed

Shutter Blockout Open

Shutter Shade Open

Shutter Shade Closed

If you have shutters installed in your home and if you have set up a Shutter Relay widget in your smart home system, you can conveniently open or close the shutters with a tap on the widget.

If you want to let in natural light in the morning, you can use the widget to open the shutters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.