D3349890_04

Local Scene Controller

Local Scene Controller widget is used to control and management of various smart home or building automation functions within a scene.

Local Scene Controller allows multiple lights to be set to predetermined levels all at once, and also allows the levels to be nudged up/down.

The functions supported by the widget are:

  • Set scene

  • All On/Off

  • Nudge up/down

To operate the Local Scene Controller:

  1. Click Set Scene to trigger the scene.

  2. Click All On/All Off buttons in the widget to turn On/Off all objects in the scene.

  3. Use ˄ and ˅ buttons to operate the nudge value.

On State

Off State

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.