D3349890_04

Bellpress

The Bellpress widget is used for momentary activation of a load, for example a doorbell.

The function supported by the widget is:

  • Bellpress

To operate the Bellpress:

  1. Click anywhere on the widget to activate it.

Off State

On State

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.