D3349890_04

Introduction

NOTICE
PRODUCT COMPATIBILITY NOTICE WITH 5500NAC2/AC2 FIRMWARE 2.0.0 and above
There are compatibility issues with the 5000ETP10W Ethernet Touch Panel running on different Android versions, refer below for more info:
  • The Old 5000ETP10W Ethernet Touch Panel running Android 4 will not support the Manager UI or its associated functions.
  • The New 5000ETP10W Ethernet Touch Panel running Android 12 does support the Manager UI and its full functionality.
Firmware version 4.0 for the 5000ETP10W has introduced the Android 12 operating system, enabling compatibility with the Manager UI. Refer the screen shot below for more details.
Additionally, always back up your controller projects before updating to a newer firmware version. Projects updated to operate on firmware version 2.0.0 and above cannot be downgraded to operate on earlier versions of the controller firmware.
Failure to follow these instructions can result in an unrecoverable situation where the 5000ETP10W Ethernet Touch Panel cannot operate with the controller.

To check firmware version on your Ethernet Touch Panel:

To access the Information screen, press and hold all four corners of the touch panel for more than 10 seconds to open the Settings page. Go to Information>Firmware version.

NOTICE

AUTHENTICATION METHOD CHANGES
Starting with C-Bus Controllers (5500NAC2/5500AC2) Firmware version 2.0.0 and above, the authentication method has been updated to enhance cybersecurity. Upon upgrading to version 2.0.0, users will be required to log in after the initial upgrade.
To avoid authentication pop-up from appearing for the selected duration, check the Remember username and password check box, and then select the duration from the User cookie expiration days drop-down. By default, the user session expiration is set to 30 days and can be extended up to 365 days.
Benefits:
This change significantly improves the cyber security posture of your system, helping to mitigate unauthorised access and ensuring compliance with modern security standards.
Considerations:
As a result of this enhancement, users will need to remember that controller password and re-authenticate when duration expires.
Failure to follow these instructions can result in the device not operating properly.
NOTICE

INCOMPATIBLE EQUIPMENT NOTICE WITH OLD 5000ETP10W ON ANDROID 4
The 5000ETP10W Ethernet Touch Panel does not support the new secure authentication mechanism introduced with firmware version 2.0.0 to 2.1.0 leading to the following issues.
  • Auto Login to Visualization (PC/Tablet) pages with a defined username and password does not work, resulting in a prompt for username and password entry, blocking user access. The login prompt may occur at anytime during normal operation of the project.
  • The Controllers Landing page does not display all elements correctly.
Failure to follow these instructions can result in an unrecoverable situation where the 5000ETP10W Ethernet Touch Panel cannot operate with the controller.

This document outlines the setup for the Manager and Manager Config applications for SpaceLogic C-Bus Application Controllers.


Manager Config

Manager Config is a powerful configuration tool designed to enable system integrator to tailor your home automation experience. It provides a visual representation of the layout of your home, allowing you to define the structure and contents of your home environment which will be visible in the Manager application.

With Manager Config, you can:

  • Define Your Home’s Layout: Create a detailed representation of your home by outlining buildings, floors, and rooms.

  • Customize Visuals: Choose names, descriptions, and icons for each part of your home, enhancing the user experience and making navigation intuitive.

  • Set Up Control Items: Specify which items to monitor and control in each location, including lighting, climate, fountains, and other load types.

  • Integrate Services: Define additional services like security to achieve a comprehensive home automation setup.

By setting these parameters in Manager Config, you establish a personalized and organized framework that will be integrated into the Manager application.

The Manager Config application enables the creation of a visualization layout for floors, each containing multiple rooms.

Manager

The Manager application is your go-to interface for managing and controlling your Home Automation system. It provides a user-friendly platform to interact with the home environment defined in Manager Config.

Key features of the Manager application include:

  • Intuitive Control Panel: Access and manage all controllable items defined in Manager Config with ease.

  • Real-Time Monitoring: Keep track of your home’s lighting, climate, and other systems in real time.

  • Customizable Views: Navigate through your home layout as you defined it, with the ability to quickly adjust settings for specific rooms or areas.

  • Enhanced Security Features: Monitor and control security services to maintain the safety and security of your home.

Together, Manager Config and the Manager application create a seamless home automation experience, allowing you to customize and control your living space effectively.

The widgets can be organized using the layout of their home to define the floors, rooms and locations of each widget.

NOTE: The Manager/Config application comes pre-installed on the 5500AC2 after upgrading to v2.0.0/v2.1.0 and above. However, it is also possible to install the Manager/Config application on the 5500NAC2.

For details on how to install Manager/Config modules for 5500NAC2, refer Installing Manager/Config Application into 5500NAC2.

NOTE:
Term widget in the context of the Manager/Config and Mobile app:
A widget is a visual representation of functions or automations within the Manager application. Configured using the Manager Config app, these widgets appear in the Manager app/interface, allowing end users to control and monitor the real-time status of lighting and other load types.

System Prerequisites

PC/Tablet/Desktop:

  • Operating Systems: Windows 10 or later, Android 13 or later, iOS 17 or later

  • Minimum 4GB RAM

Browsers:

  • Google Chrome (preferably version 127 or later)

  • Firefox (preferably version 129 or later)

  • Microsoft Edge (preferably version 127 or later)

Display Resolution:

  • Minimum: 1024 x 768

NOTE: The web page may work for older devices and browsers, but it has not been verified, and we cannot assure that it will function correctly.

Getting Started

The Home page of the application controller is shown below:

Icons

Description

Set the theme and language.

Filter the apps

To unlock and rearrange the apps position.

Configure the apps

Edit the user view

Admin

User

Below table shows the feature/widgets supported in Configurator, Manager, Manager Config and Mobile App.

Feature

Configurator

Manager

Manager Config

Mobile App

Timer

Yes

Yes

Yes

Automations

Yes

-

Schedulers

Yes

Yes

Widgets

Manager

Manager Config

Mobile App

Alarm Panel

Yes

Yes

Yes

Light Switch

Yes

Yes

Yes

General Switch

Yes

Yes

Yes

Socket Switch

Yes

Yes

Yes

Lighting Preset

Yes

Yes

Yes

General Lighting Timer

Yes

Yes

General Lighting Dimmer

Yes

Yes

Yes

Lighting Status

Yes

Yes

Yes

Fan Controller

Yes

Yes

Yes

Fan Switch

Yes

Yes

Yes

Air Conditioner Swicth

Yes

Yes

Yes

Info 1

Yes

Yes

Yes

Info 2

Yes

Yes

Yes

Bellpress

Yes

Yes

Yes

Enable Preset

Yes

Yes

Yes

Two-State Enable

Yes

Yes

Yes

Change Over Relay

Yes

Yes

Yes

Shutter Relay Horizontal

Yes

Yes

Yes

Shutter Relay Vertical

Yes

Yes

Yes

Local Scene Controller

Yes

Yes

Yes

Scene Trigger

Yes

Yes

Yes

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.