D3349890_04

Home Page

All the C-Bus devices displayed in the Home page, are configured in the Manager application. Once you login to the Clipsal C-Bus manager mobile app, the Home screen is displayed.

Overview of the elements on the Home screen:

A

Home

Tap to view the Home screen.

B

Devices in a Room

Tap a device to open the device control screen.

C

Settings

Tap to access the settings screen.

D

Room Settings

Tap to rearrange the room list.

E

Device Status

Quick information about the devices in a room.

F

Automation

Tap to set up moments.

G

Security

Visible only if your Alarm Panel is connected to the controller. Tap to set up security.

NOTE: You can tap the controller drop-down at the top center of the screen to view the list of available controllers displayed at the bottom.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.