D3349890_04

Installing the Clipsal C-Bus Manager Mobile Application

Prerequisite for iOS device:

  • Requires iOS 13.4 and higher


Prerequisite for Android device

  • Android 10.0 or higher


To download from the device:

  1. Use the search term Clipsal C-Bus Manager Mobile App.

  2. Install the Clipsal C-Bus manager mobile app on a mobile phone to commission and work with the C-Bus Controller and devices.

    NOTE: The Clipsal C-Bus Manager mobile app uses your device’s browser for user authentication processes such as login, new user registration, and password reset. The app supports only Safari, Chrome, and Microsoft Edge. Confirm that one of these browsers is set as your default browser in your mobile device settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.