D3349890_04

Change Over Relay

The Change Over Relay widget is designed to perform the actions of opening, pausing, and closing electric curtains, blinds, and shutters. It provides control over these functions, allowing for efficient management of the connected devices.

  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the Change Over Relay.

  3. Tap on the widget's label. The Change Over Relay screen appears.

    • You can control the open/pause/close functions.

    • Tap to pause the curtain.

    • Tap to close the curtain.

    • Tap to open the curtain.

Open State

Paused State

Closed State

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.