D3349890_04

Local Scene Controller

The Local Scene Controller widget is used for controlling and managing various smart home or building automation functions within a scene.

The Local Scene Controller allows you to set multiple lights to predetermined levels all at once.

  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the local scene.

  3. Tap on SET SCENE to trigger the scene. The values in the controller will be set accordingly.

On State

Off State

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.