D3349890_04

Fan Switch

Fan Switch widget is used to switch fan On and Off.

The functions supported by the widget are:

To operate the Fan Switch:

  1. Click anywhere on the widget to turn On/Off.

On State

Off State

Example: You can use the Fan Switch widget to turn off the fan when they leave the house and turn it back on just before they return. This way, you can save energy and still come back to a cool home.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.