D3349890_04

Info 1

Info 1 widget is used to display date, time, RGB, unsigned integer, signed integer, floating point, and boolean details (values or data of the object assigned).

To configure Info 1:

  1. In General tab, enter the Title of the widget, Text 1 and Text 2 description.

  2. In Objects tab, select the Text 1 and Text 2 objects for the Info 1 from the drop-down.

    Info 1 supports the following type of object:

    • User Parameter

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

    NOTE: If you are using floating-point values and want to display decimal places, configure the Widget Visualization Parameters on the object to display the desired number of decimal places. If the decimal places are not configured, the mobile app will not be able to display the values accurately.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.