D3349890_04

Local Scene Controller

The Local Scene Controller widget enables the control and management of various smart home or building automation functions within a scene.

Local Scene Controller allows multiple lights to be set to predetermined levels all at once, and also allows the levels to be nudged up/down.

To operate the nudge value use ˄ and ˅buttons.

  • The predefined scenes can be enhanced using nudge up/down option.

  • All objects in the scene can be turned On/Off using All On/All Off buttons in the widget.

    NOTE: You cannot perform mixed function with the nudge buttons.

To configure Local Scene Controller:

  1. In General tab, enter the Title of the widget, and select the check box for Nudge value options.

    The Nudge value enables you to specify the percentage for the nudge action.

  2. In Objects tab, select the Trigger Object and Scene for the Local Scene Controller from the drop-down.

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

NOTE: The mobile app renders Scene behavior based on the configuration stored in Manager, not from the Scene definition in the Configurator. If the action selector of a Scene is modified in the Configurator after a Local Scene widget is created, the change does not automatically reflect in the mobile app. To apply the updated action selector, re-save the corresponding Local Scene widget in Manager Config to refresh the configuration used by the mobile app.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.