D3349890_04

General Lighting Timer

The General Lighting Timer widget is used for switching On a load for a specific period.

The functions supported by the widget are:

  • Start

  • Stop

To operate the General Lighting Timer:


  1. Click Start/Stop to start/stop the timer.

    The first click starts the timer and the second click stops the timer. Once the timer is stopped, the return value is set.

NOTE: If left running, the return level will be set at the end of the period using the ramp rate (if defined).

Timer Off State

Timer On State

Example: General Lighting Timer can be used to turn on the corridor lights for 3 hours, and then turn off.

NOTE: The Mobile application will not support the General Lighting Timer, this feature is limited to the Manager interface.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.