D3349890_04

Lighting Status

The Lighting Status widget displays the current status of a specific light (whether the light is on, off, or in any other state).

Example: You can configure Lighting Status widget to check if the garage lights are off before heading to bed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.