D3349890_04

Before Installing Clipsal C-Bus Manager Mobile App

After fulfilling the following requirements, you can start installing and setting up your mobile application:

Action

Description

Running C-Bus installation

The C-Bus devices have been installed and set up by a system integrator.

C-Bus controller installed

The controller fulfills the hardware and firmware requirements mentioned in chapter Prepare the Controller. The controller has been properly set up, the C-Bus project has been imported into the controller.

Manager visualization created

See more in Creating Manager Visualization.

  • Manager is a widget based visualization that provides easy control over C-Bus devices in the installation.

    In a few steps, the system integrator creates the building structure (floor and rooms), they add specific widgets and select the required C-Bus group objects depending on the function the widget is controlling.

    Upon creation, widgets will seamlessly generate visualizations within the Clipsal C-Bus manager mobile app, with the flexibility to add widgets at any point in the Manager. Furthermore, the widgets are automatically synchronized with the Clipsal C-Bus manager mobile app.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.