D3349890_04

Shutter Relay Horizontal

Shutter Relay Horizontal widget is used to operate electric curtains, blinds, and shutters.

The functions supported by the widget are:

It has dual-control functionality which enables to handle both blinds and shades together. Shutter and blinds can be controlled individually using slider.


To operate the Shutter Relay Horizontal:

  1. Click (<) and (>) buttons to open/close the shutter and blinds.

  2. To control the blockout and shade together, use the dual control.

Dual state off

Dual state on

Shutters and blinds controlled individually using slider

Example: You have shutters installed in your home and you have set up a Shutter Relay widget in your smart home system. Using this widget, you can conveniently open or close the shutters with a simple tap on the widget.

For instance, if you want to close the shutters in the evening for privacy and security, you can use the Shutter Relay widget to send a command that closes the shutters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.