D3349890_04

Change Over Relay

The Change Over Relay widget is designed to perform the actions of opening, pausing, and closing electric curtains, blinds, and shutters.

The functions supported by the widget are:

  • Open

  • Pause

  • Close


To operate the Change Over Relay :

  1. Click the ˄ and ˅ to open, pause, and close the curtain.

Open State

Paused State

Closed State

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.